Skip to main content
Associate
July 28, 2025
Question

TIM1 (125 Hz PWM) to trigger TIM8 only on PWM falling edge

  • July 28, 2025
  • 2 replies
  • 305 views

Hi everyone,

I’m trying to chain two timers on an STM32U585 so that:

  • TIM1 generates a PWM on PA8 at 125 Hz (2 ms high / 6 ms low).

  • TIM8 acts as a 20 µs sampler: it should reset and start counting at the falling edge of the TIM1 PWM, then fire its Update IRQ after 20 µs.

So far I’ve tried: 

// TIM1: 125 Hz PWM at 160 MHz / APB2
htim1.Init.Prescaler = 319; // 160 MHz/320 = 500 kHz → 2 µs tick
htim1.Init.Period = 3999; // 4000×2 µs = 8 ms → 125 Hz
// …
TIM_MasterConfigTypeDef mcfg = {0};
mcfg.MasterOutputTrigger = TIM_TRGO_OC1REF; // TRGO on CCR1-match (PWM falling edge)
HAL_TIMEx_MasterConfigSynchronization(&htim1, &mcfg);
// TIM8: 20 µs sampling, slave-reset on TIM1_TRGO
htim8.Init.Prescaler = 159; // 160 MHz/160 = 1 MHz → 1 µs tick
htim8.Init.Period = 19; // 20×1 µs = 20 µs sample interval
// …
TIM_SlaveConfigTypeDef scfg = {0};
scfg.SlaveMode = TIM_SLAVEMODE_RESET;
scfg.InputTrigger = TIM_TS_ITR0; // ITR0 = internal TIM1_TRGO
HAL_TIM_SlaveConfigSynchro(&htim8, &scfg);
HAL_TIM_Base_Start_IT(&htim8);

 

However, TIM8 still resets on the rising edge (timer overflow) of TIM1, not the falling CCR1 match. I’ve checked RM0456’s “Internal trigger connection” table and ITR0 really maps to TIM1_TRGO, but internal triggers apparently only detect rising edges. I also tried using ETRF (external trigger) but could not get PA8 routed to TIM8_ETR easily.

My question:

  1. Is there a way to make TIM1’s TRGO output respond to the PWM falling edge and have TIM8’s Slave-Reset on that falling-edge signal?

  2. If I must use an external pin or IC channel, which registers / HAL calls do I need so that TIM8 will reset precisely on the High→Low transition of TIM1_CH1?

Any example code or register-level guidance would be hugely appreciated!

Thanks in advance,

Dave

2 replies

waclawek.jan
Super User
July 28, 2025

> TIM8 still resets on the rising edge (timer overflow) of TIM1

How do you know?

Isn't TIM8 free running?

Read out and check/post content of TIM1 and TIM8 registers.

JW

Technical Moderator
July 29, 2025

Hello @ProNet36 

Sensitivity can't be configured on internal triggers (ITRs). always sensitive to a rising edge (or high level as per selected slave mode.)

Possible workarounds:

  • Option 1: output the signal on TIM1_OC1 and connect it (physically) to TIM8_ETR input. Then at TIM8 level select the ETR input as trigger of the slave mode controller. It is also possible to connect TIM1_OC1 to TIM8_TI1 (channel 1 configured as input) and then select tim_ti1f_ed as trigger of the slave mode controller
  • Option 2: change the polarity of TIM1_OC1 output.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"