Timer instance not working in FreeRTOS context
Hello all, I explain you my problem the best I can.
I have a project with the MCU STM32U575RGT6 The project has TouchGFX and FreeRTOS. After the initializations of the peripherals, I have the next calls, so the while(1) in main.c is not executed. As you can see in the next image.

So for the moment the only main loop I have detected in the application is the timer interruption.

In CubeMX I have 3 timers defined: TIM17, which is been assigned to the system as the timebase source:

And timers 2 and 4 with the same exact parameters in CubeMX: (timer3 is related to an encoder....)



I initialize the corresponding interruptions.

The problem is that in the interruption HAL_TIM_PeriodElapsedCallback I never get the call of the timer 4 instance.

Any help will be welcome.