Skip to main content
VKoen.1
Associate
September 10, 2024
Solved

USB CDC in STM32H563

  • September 10, 2024
  • 3 replies
  • 1402 views

tried to set up a USB device serial emulation (CDC) for STM32H563. Started a Free RTOS based project project in STM32CubeMX. But there I only can activate USB as "device_only in the "connectivity" segment but do not find any other USB related settings. I did that previously with the stm32F series and there it was in STmCube, no prob.

The generated code also seems not to have the USBD_DESC_Private_Defines or similar things needed. 

Is it somewhere hidden under another name in STM32Cube? Or does STM32Cube does not support it? Or is this  CPU issue? Or do I need to somehow get me drivers from other places and when yes, from where?

 

 

Best answer by VKoen.1

Just to close this topic:

 

I got it running on a stm32H563 following STM advice

https://community.st.com/t5/stm32-mcus/how-to-use-stmicroelectronics-classic-usb-device-middleware-with/ta-p/599274

 

The only weak point was, that I had to switch off the ICACHE, probably because of a weakness in the STM code concerning read out of CPU serial number, but I did not need the speed, and so I was good

3 replies

AScha.3
Super User
September 10, 2024

You are invited, to use Azure /ThreadX . :)

 

Here (threadx activated) you can choose ... :

AScha3_0-1725975678881.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
lbthomsen
Associate
August 8, 2025

Well, I for one will politely decline that invitation.

Technical Moderator
September 10, 2024

Hi @VKoen.1 

Which USB stack do you want to implement? If you are using ST Library stack, it is not implemented in CubeMX. You can check examples provided here.STMicroelectronics/stm32h5-classic-coremw-apps: Provide a set of applications for STM32H5xx series based on the STM32 Classic Core Middleware libraries. (github.com)

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
VKoen.1
VKoen.1AuthorBest answer
Associate
August 8, 2025

Just to close this topic:

 

I got it running on a stm32H563 following STM advice

https://community.st.com/t5/stm32-mcus/how-to-use-stmicroelectronics-classic-usb-device-middleware-with/ta-p/599274

 

The only weak point was, that I had to switch off the ICACHE, probably because of a weakness in the STM code concerning read out of CPU serial number, but I did not need the speed, and so I was good