Skip to main content
Visitor II
July 18, 2025
Question

USB Host on STM32H755ZI-Q: CDC Class Not Detected for USB-to-TTL Device

  • July 18, 2025
  • 1 reply
  • 221 views

Hello ,

I am working with the STM32H755ZI-Q board and configuring it as a USB Host. I’ve successfully tested the USB Host functionality using standard USB devices such as a keyboard and a mouse, both of which are recognized correctly by the host.

However, when I connect a USB-to-TTL adapter to the host, it fails to detect or enumerate the device. There is no response or indication that a USB device has been connected.

I would appreciate any guidance or suggestions on the following:

Are USB-to-TTL adapters supported in USB Host mode by default?

Is there any specific configuration or class driver (e.g., CDC class) that I need to enable for this to work?

Has anyone successfully interfaced a USB-to-TTL device with STM32 USB Host?

This is the output I see on Tera Term after enabling the user log :

USBH Event Triggered
Event : Start
PID: 7523h

VID: 1a86h

Address (#1) assigned.

Manufacturer : N/A

Product : USB Serial

Enumeration done.

This device has only 1 configuration.

Default configuration set.

No registered class for this device.


What steps are required to enable CDC functionality when connecting a USB-to-TTL adapter to the STM32 USB Host?

1 reply

Technical Moderator
August 4, 2025

Hi @Akshay_S 

> Are USB-to-TTL adapters supported in USB Host mode by default?

No, USB-to-TTL adapters are not supported by default unless the USB Host stack includes the appropriate USB CDC ACM. Did you check this this knowledge base article?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL