Skip to main content
Associate II
July 24, 2025
Solved

USBH_AUDIO_InputStream() missing — how to stream USB microphone data on STM32?

  • July 24, 2025
  • 1 reply
  • 407 views

Hello,

I'm working on a project using the STM32F401RE board to perform real-time fault diagnosis on machinery.
The board receives vibration data in real-time via a USB-type accelerometer (Digiducer 333D01), and a lightweight deep learning model running on the MCU determines whether the signal indicates a normal or faulty condition.
All of this is running under FreeRTOS and must meet real-time constraints.

The accelerometer is connected through a USB breakout board (YwRobot ELB050209), and the STM32 board is configured to operate as a USB Host with Audio Class support.
The USB connection and device enumeration process (including descriptor parsing) have been completed successfully.

Interestingly, the Digidecer 333D01 is recognized as a USB Audio Class device, specifically as a microphone-type interface.
The device presents itself with an Audio Control interface and an Audio Streaming interface (Isochronous IN), similar to a standard USB microphone.
Although the data represents vibration (acceleration) rather than audio, it is transmitted as 24-bit PCM over isochronous transfers, just like microphone audio data.

The problem I'm facing is in the next step: receiving streaming data from the device.
I found that the function USBH_AUDIO_InputStream() is declared in the STM32CubeMX-generated code, but it is not actually implemented.
Therefore, I’m looking for any example code, application notes, or sample projects that demonstrate how to receive data from a USB microphone (or any isochronous IN Audio Class device) using STM32 as a USB Host.

Any references or advice would be greatly appreciated.
If more information is needed, I’d be happy to provide it.

Note: This message was written using a translation tool, so I apologize in advance if any part sounds unnatural or unclear.

Thank you!

Best answer by FBL

Hi @SR1218 

Have you checked this example

1 reply

FBLBest answer
Technical Moderator
August 5, 2025

Hi @SR1218 

Have you checked this example

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL