Skip to main content
Senior
April 24, 2026
Question

using M95P32-I with custom stm32-mw-extmem-mgr

  • April 24, 2026
  • 2 replies
  • 86 views

I would like to use some of your 

 

The problem is that i don't understand how to use your memory loader with these chips

 

 

The problem is that this library expects the chips to have 4 byte address and just doesn't work with 3 address chips.  If you go through and just change all the call's to 3 byte address in the library i can make a STLDR file to talk to the chip.  Just trying to see if there's a better way. 

 

You have this custom memory section that would help i just don't know how to use it?  So i'm hoping for some help there.

 

2 replies

Technical Moderator
April 24, 2026

Hello @Brenden_PLUS 

The better way is not to change the whole loader from 4-byte to 3-byte addressing everywhere. Instead, keep stm32-mw-extmem-ldr as the loader framework and create a small device-specific low-level driver for your EEPROM where the address length = 3 bytes is handled in one place.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Senior
April 24, 2026

I'm not sure what your suggesting.

 

I want to use the "stm32-mw-extmem-ldr as the loader framework".  The problem is that it just can't do 4 byte address.  For my program i have support for the chip, since i'm using zephyr. 

 

The problem is i don't have a way to program the board.  ST programmer using STLDR files and the sudgested program to use to make the STLDR for the N6 and H7 is stm32-mw-extmem-ldr.  It works good just not for the smaller parts.  There are custom parts in the repo.  I just don't know how they are used.  In that custom directory they have parts that start off with 3 byte address.  I just don't know how to enable it.  

ST Employee
April 27, 2026

Hello @Brenden_PLUS , 

 

You do not need to patch the custom extmem manager globally to force 3-byte addressing as you have noticed. The custom layer already exposes AddressSize, and the normal command path uses EXTMEM_CUSTOM_ADDRESS_24_BITS correctly. For a standard serial page EEPROM, the useful adaptation is to describe the part as a custom EEPROM memory in a dedicated template file under memories folder, keep the access mode in 1S-1S-1S, set the read/write/status opcodes from the datasheet, and let the manager reuse the existing page-write plus WIP/WEL polling path. The only extra change needed is to avoid NOR-flash erase commands, because EEPROM writes do not require sector erase.
 
Kind regards, 
DHIF Khaled
"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"