Skip to main content
Associate II
May 19, 2025
Question

Write sd timeout,the restart code does not take effect

  • May 19, 2025
  • 1 reply
  • 644 views

The reason is that the update of the HAL library caused the SD card problem, which led to bus_hault after the restart. The SD card will only be restarted when there is a read/write issue. The reset process is deinit followed by init.

Kaitou_0-1747623088854.png

Later, it was found that DPSM was an unexplainable setting, causing the driver to believe that there was data directly read from the fifo, but the data program was written to DPSM in conjunction with SDMMC_CK.

Then I changed the driver code to seem to have solved the problem, and restarted the code by adding abort before deinit and init.

Kaitou_1-1747623103137.png

1、Why does the SD card often malfunction? Is it caused by the clock waveform? Is this waveform setting incorrect for DPSM?
I adjusted the frequency to 4M, but the Voltage overshoot was very large.Yellow represents CK and pink represents 3.3V voltage

Kaitou_2-1747623125751.pngKaitou_3-1747623133605.png

2、I used a soft restart for the SD card, but it seems to be of no use. Is there a way to solve the problem of the SDMMC getting stuck at a certain state due to being stuck at the DPSM?

If the abort continues, it will cause the IDMA to step on other stack Spaces, thereby resulting in a hardfault.So if abort fails once, I won't use the SD card anymore.

Kaitou_4-1747623154295.png

When there is a problem with the SD card, it will keep waiting for the flag bit. The same is true of reinitialization

Kaitou_5-1747623167553.png

Thank you for your help.

1 reply

AScha.3
Super User
May 19, 2025

>1、Why does the SD card often malfunction?

Probably a hardware problem.

 

- How long are wires/connection from cpu pin to sd-card ?

- pin speed you set ?

- clock for sdmmc is ..? MHz

- DMA used ? (Tried without DMA ?)

"If you feel a post has answered your question, please click ""Accept as Solution""."
丶KaitouAuthor
Associate II
May 19, 2025

The cable from the CPU to the sd card is 32.9MM long

SDMMC_CK is 4Mhz

IO speed is GPIO_SPEED_FREQ_MEDIUM

yes,i use dma;I didn't try not to use dma

AScha.3
Super User
May 19, 2025

33mm should be fine. (Is really from cpu-pin to card-pin ? or from board to card ?)

So try first:

- all pins speed medium + pullups ON

- sdmmc clock 50MHz  (i use 100M and div 1 -> 50M )

- 1 bit mode

- no DMA

-> init , wait 50ms (hal-delay) , many cards need some time for internal init,

and then only mount (parameter 1 , = now ) and read (from any existing file on card), use "good" card (e.g. SanDisk).

THIS has to work perfekt .

Then we go on...  ok ?

"If you feel a post has answered your question, please click ""Accept as Solution""."