About board EVSPIN32G4
Hello, I need help the product I mentioned EVSPIN32G4 I've been trying for a long time to find the pins on the board to control GPIO signals instead of SPI Interface
I need to find these pins on the board:
I/O control terminal
GND Ground wire
F/R Forward and reverse
EN Start Stop
BK Brake Control
SV Analog input
PG Speed pulse signal output
ALARM Alarm output
+5V Speed regulation voltage output
STSPIN32G4, this is the chip of the board found in EVSPIN32G4
This is the link for the EVSPIN32G4: https://www.st.com/en/evaluation-tools/evspin32g4.html
And that of the STSPIN32G4: https://www.st.com/en/motor-drivers/stspin32g4.html
I use external microcontroller with firmware to control the motor driver its for cnc axes movement application
Regarding the I/O control terminal I mentioned, I don't see that there are exactly the same as in the list I mentioned above, just maybe someone can help me find these pins according to the Block Diagram of the STSPIN32G4
Thanks for help!