Skip to main content
駿茂手木.1
Associate
July 1, 2022
Question

About project generation at "st motor control workbench"

  • July 1, 2022
  • 2 replies
  • 882 views

I would like to ask a question about "st motor control workbench".

When I generate the sample project of STEVAL-SPIN3204, I get the following error.

I want to solve this error.

If anyone has been in the same situation and was able to solve it, please help me.0693W00000QKG3eQAH.png

This topic has been closed for replies.

2 replies

Dane._.T
Associate II
July 1, 2022

I got it to generate on MotorControl Workbench 5.4.8 with the following settings:

STM32CubeMX - 6.5.0

Target Toolchain - ST STM32CubeIDE

Firmware Package Version - STM32 FW V1.11.3

You also may have clicked the "Generate" button. Sample projects usually require clicking the "Update" button to work properly.

駿茂手木.1
Associate
July 4, 2022

0693W00000QKMfUQAX.pngThanks for replying. I am working in this environment right now.

STM32CubeMX - 6.6.0

Target Toolchain - ST STM32CubeIDE

Firmware Package Version - STM32 FW V1.11.3

I have successfully generated the code with the "update" button. However, I am unable to build the project.

I was able to build when I hit the "generation" button to generate code for a different board, but were you able to build yours?