ADC issue STM32H723ZG with IHM08M1
Hi all,
I'm in the process of configuring my STM32H723ZG to work with the IHM08M1 motor driver shield.
Currently I am trying to configure and validate the signals from the ADCs however I am having some issues with this. One ADC I'm trying to validate is the DC voltage bus reading. This circuit simply places the input through a voltage divider with some protection, going straight to the ADC after. I've tried configuring these ADCs in a few different ways, single channel, DMA, etc. however none of them produce the expected results.
What I'm currently seeing is that with the stm and shield disconnected, I can read the correct stepped down voltage on the shield side by probing with a multimeter (~0.5V depending on input voltage). When the stm is disconnected to the shield the ADC reads a floating ~1.64 volts. With the two connected the ADC seems to still be reading 'garbage' values, probing with a multimeter reads ~1.75 volts. The last bit of information I have is that by grabbing on to the ADC pin directly I am able to drive the signal to either 0V with ground or 3V3 with the stm's voltage source, and successfully read this in code.
I am relatively new to STM's so i appreciate you taking the time and effort to help me, any and all feedback is welcome.
Thanks