Associate III
December 30, 2023
Question
Adding a custom boards to MotorControl Workbench 6.1.1
- December 30, 2023
- 3 replies
- 5621 views
Hello all,
I have developed a custom control board and a custom power board. I am trying to add them to MotorControl Workbench 6.1.1 and I have written a custom JSON files describing both board. A few interesting things:
I am using STM32G431RBT6 as my MCU, the NCP51820 is gate driver and the current is measured with ACS772ECB hall effect current measurement IC. And the this is how it is connected to the MCU, most important connections are marked in red.

I am getting
Error
The hardware selected is not compliant with the selected algorithm. Please review your selections.
When I try to start a project. I have made a two decisions because I did not know what else to do.
The first is I can't see how to add e custom connector, so I used MotorControlConnector type.
The second is I can't see hall effect sensor type for current sensing and I chose ThreeShunt_RawCurrents_SingleEnded
Can anybody tell me what I am doing wrong? The MotorControl Workbench 6.1.1 is not very descriptive. On semantic check all is good. The JSON is valid and all of the features properties are set. Do you need any other information to help?
Can anybody tell me what I am doing wrong? The MotorControl Workbench 6.1.1 is not very descriptive. On semantic check all is good. The JSON is valid and all of the features properties are set. Do you need any other information to help?