Availability of the X-NUCLEO-IHM09M1 vs. M2
1) There is no availability of the X-NUCLEO-IHM09M1 at Mouser or Digikey. Both vendors do, however, have stock of the X-NUCLEO-IHM09M2. Has the M1 been discontinued? Please let me know if there is any difference between the M1 and the M2.
2) If it turns out that the M2 replaces the M1, does SB26 still need to be removed? It’s going to be very difficult to remove SB26 without damaging the board due to its tiny size and awkward location.
3) I also need the specs and part number on the 34 pin ribbon cable that interfaces the B-G473E-ZEST1S controller board to the STEVAL-IPM30B evaluation board.