B-G431-ESC1 Battery Measurement source code error in conversion factor
I am referring to the B-G431-ESC1 source code and i feel there is an error in the battery voltage measurement source code. A conversion factor is used to convert from the ADC voltage to the battery voltage. It is initialized as follows
RDivider_Handle_t BusVoltageSensor_M1 =
{
._Super =
{
.SensorType = REAL_SENSOR,
.ConversionFactor = (uint16_t)(ADC_REFERENCE_VOLTAGE / VBUS_PARTITIONING_FACTOR),
},
The voltage is read in u16Volt format when reading the ADC register value , I assume the adc driver will only give max value of 12Bit (4096) for 3.3V, but where is this conversion added to convert to Battery voltage. Please advise.