Skip to main content
Associate III
March 11, 2025
Solved

B-G431B based custom board

  • March 11, 2025
  • 1 reply
  • 370 views

I have designed a board similar to B-G431B ESC1 kit and using the FOC code from the motor control work bench. But at present i have an issue where the Gate to Source Voltage is equal to Bus Voltage (VDC) instead of the 12V. What could be the problem? The Mosfet driver IC i am using is 2ED2182S06FXUMA1.

STUser34_0-1741684605143.png

STUser34_0-1741684806737.png

 

 

Best answer by STUser34

The problem is because of the below setting in motor control work bench

STUser34_0-1741855935422.png

I have now updated to 20ms and it works i have kept the charge boot capacitor duty still to 0%, i plan to change that as well to 50%. I am not sure which value to be kept.

1 reply

STUser34AuthorBest answer
Associate III
March 13, 2025

The problem is because of the below setting in motor control work bench

STUser34_0-1741855935422.png

I have now updated to 20ms and it works i have kept the charge boot capacitor duty still to 0%, i plan to change that as well to 50%. I am not sure which value to be kept.