B-G431B-ESC1 generated missing code PWM support from 6.0.0 MC Workbenck release
Hi,
I'm testing the B-G431B-ESC1 evaluation board by using the PWM input to control your motor.
I saw that the B-G431-ESC1 is fully supported from the 5.4.1 release but I can't be able to find anymore information about the 5.Y or 6.0.0
I could get the source code with the pwm input with version 5.4.8. i could see that the pin PA15 called M1_PWM_INPUT is present in your cubeMX file
On the other hand, I could not establish how to change the frequency to use it with a frequency of 50hz instead of 490 Hz.
I tested it anyway and the engine armed and turned but with a great instability.
In view of the improvements present in version 5.Y and 6.0.0 and the support of the FOC, I would like to know if I can get a code with the support of the pwm input?
I have already tried to take the example code from version 6.0.0 of MC Workbenck but the implementation of the pwm input is not present.
Kind Regards,
Anthony