B-G431B-ESC1 over current fault after setup.
I was able to run the ST MC Workbench tool
for motor and parameter configuration successfully and the motor ran fine. I then uploaded the generated code through STM32CubeIDE however once uploaded when I try to start the motor there is an audible click from the ESC and MC workbench an over current fault is shown.
The motor ran fine in the motor profiler and did not show a fault.
In the MC workbench overcurrent is turned off in the power stage. In the control stage I increased the current threshold and it was unsuccessful also.
If you need any other info please say thanks