B-G431B-ESC1 Overcurrent
Hi everybody,
First of all I don't have experience in FOC.
I have profiled the motor, and the procedure was succesfully completed.
I use the motor profile to create a FOC project.
When I try to start the motor using the Motor Pilot an Overcurrent Error appen (in both mode speed and torque).
Now in normal motor drive the closed current loop regulate the 3-phases motor current by monitoring the current and comparing it to the setpoint created with torque reference respect
to the electrical motor angle, this means that if no short circuit is present, is not possible to get Overcurrent error.
Now in FOC the electrical angle before the motor start must be generated in some way that is not clear to me.
I try to change some paramiter as suggested in the help of Overcurrent error, but nothing change.
Any try give always Overcurrent error.
Using an osclilloscope to investigate, no current flow to the motor phases but systems give this error.
Board is ok because with 6 step methode everything work correct.
Can someone suggest something ?