b-g431b-esc1 Overcurrent at the start
I have a custom motor controlled with the b-g431b-esc1 that I have been able to run in position control mode without overcurrent protection. As soon as I activate overcurrent protection the motor goes in the fault state when I click the "start" of the motor pilot. The motor does not perform even alignement. I tried to change the following lines of code of `mc_parameters.c` file:
```
const R3_2_Params_t R3_2_ParamsM1 =
{
.....
/* DAC settings --------------------------------------------------------------*/
.DAC_OCP_Threshold = 4083,
.DAC_OVP_Threshold = 23830,
};
```
moving the `DAC_OCP_Threshold` to 4483 and the motor does not go in overcurrent anymore. I think that 4083 is generated from the MC_Workbench from the 45A limit of the board, but using the 4483 exceed the 4096 that should be the 12-bit DAC limit.
The motor is powered with a supply limited to 5A. For this reason I think 45A current on the shunt resistors is hard to be reached.
Am I missing something?
Let me know,
best regards