B-G431B-ESC1 with MCSDK 6.4.1: Cannot generate or find Motor Profiler firmware.
Hello,
I am using the B-G431B-ESC1 board with a fresh installation of X-CUBE-MCSDK-6 (v6.4.1).
I want to use the Motor Profiler, but I am facing a problem:
1. The precompiled profiler firmware (.bin/.hex file) for B-G431B-ESC1 is not included in the 'Utilities' folder. I understand this may be by design in newer SDKs.
2. However, when I create a "New Project" in MC Workbench and select the B-G431B-ESC1 board, the option to create a "Motor Profiler" firmware does not appear. Only the "FOC" option is available.
Because of this, I am completely stuck and cannot run the Motor Profiler.
Could you please advise on the correct procedure to get the profiler firmware for the B-G431B-ESC1 on MCSDK 6.4.1?
Thank you.