Skip to main content
Raphael_Ko
Associate II
January 8, 2026
Solved

B-G473E-ZEST1S with MCSDK 6.4.1 singnal handler after startup

  • January 8, 2026
  • 2 replies
  • 486 views

Hallo,
i try to run an B-G473E-ZEST1S with STEVAL-LVLP01A. I generate code with the default setting from MCSDK 6.4.1., STM32CubeMX 6.16.1, STM32 FW V1.6.1 (Recommended)

I changed nothing on the board hardware or MCSDK settings, i choose the 2 boards and generate code, but after startup I end always in an "<signal handler called at 0xffffffe9>".

The error occours after MX_NVIC_Init(); without MX_NVIC_Init(); the code is running, so it has something to do with the interrupts, but I don't get it.
Does anyone know what could be the cause of this error? Has anyone successfully used this board with the MCSDK 6.4.1?

Thank you!

Best answer by Raphael_Ko

I have found it, it was the missing boot 0 jumper on the board.

2 replies

Raphael_Ko
Raphael_KoAuthorBest answer
Associate II
January 8, 2026

I have found it, it was the missing boot 0 jumper on the board.

GMA
Technical Moderator
January 12, 2026

Hello @Raphael_Ko,

Thank you for your feedback.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA