BLDC motor control using Temperature sensor
Hi all, I have been trying to control my BLDC motor with an condition where if the surrounding temperature increases a threshold temperature the bldc motor should turn fast else slow. I am using lm35 as temperature sensor, i was able to interface this using stm32 nucleo g431rb board , esc and lm35 but i want to interface this through the code generated from motor control workbench. I need few insights on this, the code is generated for P-Nucleo-IHM03 motor control pack with FOC control algorithm.