Board Manager: difference of "features" object in an inverter board
Can you explain to me the difference between the features object inside the motorDrives object, compared to the standalone features object? Most object inside motorDrives make sense as a Feature of the motor drive itself, but not all.
We're using the B-G431B-ESC1 board JSON for reference.
For example the TemperatureSensing feature, what would happen if I put this into the standalone features object instead?
Or vice versa, with the ElectronicSpeedControl feature, why is this in the standalone features object even though it is directly related to the motorDrives functionality?
I cannot make sense of the logic behind this right now.