Can I control a BLDC motor based on encoder counts?
Hello.
I'm using Nucleo F446re and IHM07M to control a BLDC motor. It has a built-in 2000 pulse quadrature encoder. The MCSDK version is 5.4.8. I tried the position control method and it works fine. However, it only allows me to control the motor based on the provided angle in radian. For a specific purpose, I need to control the motor based on the number of counts it crossed. Is there a way to do that?
Regards,
Sihab