Skip to main content
TKara.2
Associate III
December 21, 2024
Solved

Can i use motor pilot with custom board

  • December 21, 2024
  • 1 reply
  • 956 views

I can use a motor profiler with a custom board, but can I use a motor pilot with the same software? Is it possible to use a motor pilot with a custom board?

 
 
Best answer by Gael A

Hello TKara.2,

Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.

1 reply

Gael A
Gael ABest answer
ST Employee
January 6, 2025

Hello TKara.2,

Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.
TKara.2
TKara.2Author
Associate III
January 7, 2025

Thanks @Gael A