Skip to main content
Visitor II
March 25, 2025
Question

Connection between B-G483-ZEST1S and STEVAL-IPM30B

  • March 25, 2025
  • 1 reply
  • 289 views

Hello!

I am trying to connect the B-G483-ZEST1S and STEVAL-IPM30B boards together for motor control. The connectors on the two boards have a different number of pins. Is there a ribbon cable that connects these? Or should these two boards not be used to evaluate the SLLIMM module?

Thanks,

DJ

1 reply

GMA
Technical Moderator
March 25, 2025

Hello @DJMcLeod,

Connection is done via X-NUCLEO-IHM09M1 adapter bridge board.
Project setup with "Control Connector" selection set to Morpho in "Connections" tab.
It is not mentioned on current MCSDK6.3.2 version but SB26 has to be removed (VBus sensing conflicting with Potentiometer feature).

GMA_0-1742924418781.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA