Skip to main content
Visitor II
April 7, 2026
Question

Connection Issue with ST Motor Pilot (Latest Version) and Dependency Conflicts with Older Versions

  • April 7, 2026
  • 1 reply
  • 106 views

I am currently working with MC Workbench and the ST Motor Pilot tool for motor control development. While setting up and attempting to establish a connection using the latest version of ST Motor Pilot, I am encountering a connection issue that appears to be caused by a bug in the current release.

As suggested in the community forums, I also tried using an older version of ST Motor Pilot. However, this introduces dependency conflicts, as other required components and tools in the workflow depend on the latest versions and are not fully compatible with the older Motor Pilot version.

Board- STEVAL-ESC001V1

 

 

1 reply

GMA
Technical Moderator
April 10, 2026

Hello @Arjun38225,

With the latest MCSDK 6.4.2 available here, it is possible to connect the MC Pilot to the STEVAL-ESC001V1 board.
For more information, refer to 2.2 Communication, programming and command interfaces chapter in the STEVAL-ESC001V1 user manual.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA