Skip to main content
frankers
Associate
July 15, 2022
Question

cubeMx with stspin32g4

  • July 15, 2022
  • 2 replies
  • 1807 views

i want to create a firmware for the stspin32g4 mcu but the cubeMx let me not select this mcu. in fact no spin mcu. i can not select a mcu with name spin

cubemx bug or st now not support the mcu with integrated drivers?

This topic has been closed for replies.

2 replies

frankers
frankersAuthor
Associate
July 15, 2022

i have cubeMx 6.5.0 on windows 10

in the IDE is the same, i can not select a spinXXX mcu

Nikita91
Lead II
July 16, 2022

As the stspin32g4 includes a STM32G431VB, you should be able to work by selecting that one.

Martin_Honig
Visitor II
February 26, 2024

I encountered the same problem, it can be used, but for HW egineer it is lacking the function of knowing your possibilites where to pin swap alternate functions etc. because you have not got the reference to avalailable pins on STSPIN32 package, you have to do a lot of workarounding to at least get an idea.