Engine stops after a few seconds.
Hello everyone.
I am using the Motor Control WorkBench 6.3.0 application to generate the project. The inverter board is
B-G431B-ESC1. The motor is a 2-pole BLDC, 8.5V, it has a very low inductance of 0.04mH, an Rs of 0.37ohms and the B-Emf constant is 0.285 Vrms/kRPM.
In the data sheet
indicates that 60,000 RPM are the maximum it can reach.
I configure the application to reach 15000 rpm. After executing the acceleration ramp, the engine stops and gives start up failure.
Could you tell me what steps I should take to keep the motor turning. I would like to get a higher speed (25 or 30 KRPM) but first I'm trying to get it to run at 15KRPM.
Project attached.
Thank you all very much for your time.