Question
Error when generating code with MC Workbench 6.3.0
- May 21, 2024
- 1 reply
- 3199 views
Hello there,
I am currently working on a project considering the B G431B ESC1 and a BLDC motor.
My goal is to control the motor through a external PWM Signal from a nucleo board.
So far I could only control the BLDC motor through the MC Profiler and only in 6Step mode.
After some research I found out that in order to control the BLDC motor with an external signal the ESC setting must be activated in the "Stage Configuration".
I did that and generated the code for the B G431B ESC1, however I recieve the following error message found in error.txt.
Some variable seems not be declared.
Any tips on how to solve this issue?
Thanks in advance
Batu