Skip to main content
Visitor II
March 15, 2024
Question

EVLDRIVE101-HPD firmware example is missing.

  • March 15, 2024
  • 1 reply
  • 2837 views

I would like to have a firmware example for EVLDRIVE101-HPD.
Do you know where I can find firmware examples for this board?

1 reply

ADAVE.1
ST Employee
March 15, 2024

Hi @JamesPark 

here's the board description file (JSON file) of the board that you can import and use to generate the code.

Alessio

John Thorne
Associate
August 1, 2024

Hi ADAVE.1

Are there any MCWB example project files available for the EVLDRIVE101-HPD?

This JSON file you published only accesses the "General Info" on the product, which is all on the ST web site. Where is the example project file? The EVLDRIVE101-HPD is not listed under "Control Board" or "Power Board" from New Project.

The nearest combination of STDRIVE101 plus STM32G071 selectable in MCWB appears to be:

EVALSTDRIVE101

NUCLEO-G071RB

X_NUCLEO-IHM09M2

but there the trail stops - "Next >" is greyed out, so we can't even port the code.

Is there an .ioc file available for the EVLDRIVE101-HPD (CubeMX doesn't recognise the EVLDRIVE101-HPD)? At least that would be a starting point.

John T.

Associate II
August 4, 2024

What version of MCWB are you using? I have it on v6.3.0.

It should be listed there. It's under "Inverter".