Skip to main content
Associate
July 20, 2025
Question

EVSPIN32F0601S1 not running motor

  • July 20, 2025
  • 1 reply
  • 260 views

Hi All,

I am trying to get up and running the above hardware. I downloaded the software for the board, and we already use IAR compiler here. After compiling and downloading (via the STLink), the system runs the program just fine.

However, I just need to run the system with the onboard POT and it is not moving or energizing the motor at all.

I changed the 6step_conf.h file to POTENTIOMETER_INTERFACE = 1 and all others to 0. Nothing happens.

All the voltages to the board are perfect (running 70VDC to the board via a 7 amp programmable power supply).

All help would be greatly appreciated. This is my first intro into using the part. Time is very tight.

regards,
Charles

1 reply

Fabrice LOUBEYRE
ST Employee
July 21, 2025

Hi SimpleStep

for using potentiometer, i suggest you first to set the potentiometer feature into the ST MCSDK WB. This will generate all the SW required to control your motor with the potentiometer. 

FabriceLOUBEYRE_0-1753091655376.png

Best regards.

Fabrice

 

Associate
July 21, 2025

Hi Fabrice,

Thank you for the information, however I am going to be using this in an embedded system and there will be no communication with the controller after the initial program is downloaded.

This is why I sent the 6step_conf.h file hoping changing this would allow me to run it without the use of the 6-step wizard.

I also need to make a connection to the system with a serial port for initial testing. After that it will not be used again expect for possibly debug info.

regards.
Charles