Skip to main content
Visitor II
July 21, 2025
Question

EVSPIN32G06Q1S3 and STLINK-V3SET not communicating

  • July 21, 2025
  • 2 replies
  • 249 views

I am working with the EVSPIN32G06Q1S3 and the STLINK-V3SET, I have the two programmer/debugger boards mounted on top of each other. Then I have the UART connector connected to the EVSPIN32G06Q1S3 (J5) and the programmer/debugger boards (CN7). I have 230 VAC going into the EVSPIN board. The lights on both the STLINK and the EVSPIN turned on. Device manager recognizes the LINK, but I can't detect the EVSPIN in Motor Pilot or STM32CubeIDE. I've tried the "Discover Board" option in Motor pilot and manually changing the baud rate to each option with no results. I think it might be a firmware issue, but I'm not entirely sure. 

2 replies

GMA
Technical Moderator
July 23, 2025

Hello @Hugo_,

With STM32CubeIDE tool, you can try to upgrade the ST-LINK version:

GMA_1-1753286794402.png

 

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
Billy OWEN
ST Employee
August 11, 2025

Hi @Hugo_ 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy