EVSPIN32G4 - current measurement burst noise at high RPM
Hi everyone!
I'm evaluating STSPIN32G4 for driving a small 6 kRPM 28-pole PMSM (up to about 30A load current - it's driving a propeller, 0.06 mH inductance, about 160 kV). Generally the performance is quite good, but I have noticed frequent STOPLL faults above a certain RPM. I tried many different tunes for the STOPLL but it didn't resolve the issue, and I went deeper.
Turns out, above a certain RPM (~5k) bursty artifacts begin to appear in current measurement (In I_A, I_B and everything "above" it) and BEMF reconstruction becomes unreliable which I think upsets the STOPLL phase detector.



This only happens:
- above a specific RPM
- on a loaded motor
- appears roughly where overmodulation starts to kick in
- the "critical" RPM after it starts to appear go down if PWM frequency is increased
I'm guessing it has something to do with the timing of current sampling (it probably samples the current at an invalid interval? or is it because of the distortion introduced by overmodulation?), and would appreciate pointers on where to dig further.