EVSPIN32G4-DUAL board takes very large current
[PN]: EVSPIN32G4-DUAL, STSPIN32G4, STDRIVE101
[VERSION]: 6.4.0
[TOOL]: Motor Control Workbench
[DETAILS]:When I start the motor from motor pilot, even though I have set low peak currents (0.2A) in the project, on startup more than 1.8A is taken from the power supply for approx 0.5s. Afterwards the current stays at 1.3A
[EXPECTED BEHAVIOR]:I would expect the current to be limited to the values specified in the design file.
[HOW TO REPRODUCE]:just start motor from motor pilot