EVSPIN32G4-Dual driver 2 motor issue
[VERSION]: MCSDK 6.2.0
[TOOL]: MC WB,
[DETAILS]: PWM output Abnormal
[EXPECTED BEHAVIOR]:M1 & M2 should drive independently & smoothly
[HOW TO REPRODUCE]:
1.Profile M1 & M2 by Motor Profiler with EVSPIN32G4. M1 & M2 got Hall .
2.Use MCSDK 6.2.0 with EVSPIN32G4-Dual to generate project(default setting, just modify Motor Hall );
3.CubeIDE compile the project & Flash into EVSPIN32G4-Dual.
4.Motor Pilot to start M1 & M2.=====first start M1 spin well.... Then spin M2-----Can see M1 stop with high frequency noise.
5.Try to spin M2 & M1 separately------Works well.
6.This EVB should be able to Drive 2 motor at the same time ,but how ?