EVSPIN32G4-DUAL I2C Pin Mapping Mismatch Between Schematic and MCSDK 6.4.1
I am currently working with the EVSPIN32G4-DUAL board and have a question regarding the I2C pin configuration.
According to the EVSPIN32G4-DUAL schematic, the I2C signals are connected to pins PC4 and PA8.
However, when generating a project using MCSDK version 6.4.1 and checking the pin mapping, the I2C interface is assigned to PC9 and PC8.
When I modify the project to change the I2C pins from PC9/PC8 to PC4/PA8 and then update the firmware image, the system does not operate correctly.
Could you please clarify the reason for this discrepancy between the schematic and the MCSDK pin configuration, and advise on the correct way to configure the I2C pins for this board?


Thank you for your support.
Best regards,
Pelino