Skip to main content
Associate
July 2, 2025
Question

Firmware error for motor profiler

  • July 2, 2025
  • 2 replies
  • 384 views

 

I am using the Nucleo-IHM17M1 and Nucleo-F401RE to evaluate a high-speed drone motor (22,000KV) with sensorless drive. I am particularly interested in the Motor Profiler function, since some key motor parameters are not provided by the manufacturer. However, whenever I open Motor Workbench with Motor Profiler (version 6.4.0) and attempt to connect, I consistently receive a firmware error message. I have reviewed the specification sheet, which confirms that these boards are supposed to be compatible. Could you suggest any possible reasons for this issue, or recommend any other compatible boards for profiling sensorless BLDC drone motors?

Thank you very much!STM.png

2 replies

GMA
Technical Moderator
July 2, 2025

Hello @uskach,

You have to generate first a project with "Motor Profiler" feature enabled:

GMA_0-1751470080066.png

 

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
cedric H
Technical Moderator
July 2, 2025

Hi @uskach,

The answer to your question is in the red Box! You need a profiler dedicated project.

You have to enable the profiler capability in the Application configuration window. 

The full description is accessible through the Workbench : About-> Documentations -> Documentation 

It opens a new navigator window, in the User Manual section, you will find the chapter Motor Profiler Application Note

 

cedricH_0-1751470157259.png

Be aware, that once your motor is profiled, you have to re-generate your project without the profiler option (but with your profiled motor) to have a fully usable project.

Regards

Cedric

uskachAuthor
Associate
July 2, 2025

Thank you for the instructions. I followed the documentation and selected a known low voltage motor similar to my application to generate the project. However, I encountered some issues during code generation. Although the project folder is still generated despite the error message, I proceeded to the IDE page.

image.png

Consequently, when I try to run the project in IDE, I encounter this error message. Do you have any suggestions or recommendations on how to generate the project without errors? Thanks a lot!

image (1).png

GMA
Technical Moderator
July 17, 2025

Hello @uskach,

You can refer to the STM32CubeIDE user manual:

https://www.st.com/resource/en/user_manual/um2609-stm32cubeide-user-guide-stmicroelectronics.pdf

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA