Hello, What is the way to use the EVALSTDRIVE601 with Motor Control Workbench 6.0.0? Best regards, Alain
A customer implemented the “EVALSTDRIVE601�? evaluation kit with a NUCLEO-G431 board.
This board combination does not exist in the "Motor Control Workbench" : the "EVALSTDRIVE601" evaluation board is not listed.
The customer started his evaluation with a "NUCLEO-G431RB" combination and a "STEVAL-IPM05F" power card, the source code of the STEVAL-IPM05F has been adapted to be compatible with the "EVALSTDRIVE601" card.
Unfortunately, it is not possible to customize the following points in the tool on the “Current Sensing�? configuration page :
• “Shunt Resistor�?
•" Gain "
In addition, the regulation management parameters of the various feedback loops seem to depend on the power evaluation card selected.
With the configuration mentioned above, he can use the “Motor Pilot�? tool but the motor is about to starts but never spin.
The customer suspects a misconfiguration of the parameters.
For the moment, he is blocked at a few configurations with evaluation boards and so he is asking :
1. Is it possible to configure the various parameters more finely, such as the value of the shunt resistors and the gain applied to the current measurement?
2. Why I can see 11 motor while creating a new MCW project whereas the customer can see only 8 motors?
3. Is there detailed documentation of the implementation of the engine library?
4. How can he configure this “custom�? hardware that he is going to develop to configure the software running on the STM32G431.
Best regards,
Alain