Question
Hi, I Use NUCLEOF446RE and X-NUCLEO-IHM08M1 for running a motor. It works for a motor with 24V power supply. But however, if I use 36V power supply and run motor profiler to estimate the parameters. It fails to rotate. Need Suggestions?
When Motor profiler is used to test the motor for its parameters, it keeps on checking with the possible current (18A, 14A, 9A, 6A, etc..). After sometime a message popup "Speed measurement takes too long time". I don't know the reason behind this. If same motor is used with 24V power supply, motor profiler works and able to run the motor using motor control workbench.