Skip to main content
Dane._.T
Associate II
June 27, 2022
Question

How can I generate an Induction Motor Control setup through MCSDK?

  • June 27, 2022
  • 0 replies
  • 813 views

Unfortunately, I cannot get MCSDK to generate the Middleware with the Induction option, as it either does not appear (v. 6.0.0) or it fails to generate pwm_curr_fdbk.c properly (v. 5.Y.4). The other two algorithms generate fine and can run my setups. From what I've seen so far, Induction seems to be newer and is only supported in 5.Y.x.

This topic has been closed for replies.