Skip to main content
DSchu.9
Associate II
July 13, 2022
Question

How can I generate an .stmcx file without the GUI?

  • July 13, 2022
  • 1 reply
  • 672 views

I have several .stmcx files to generate projects for. I don't have the time to open, generate, and wait for each one to generate. Is there a way to automate this process, preferably through Windows command line or Linux Terminal, though writing a C, C++, Python, Java, etc. is also workable.

All I need to do is generate. I do not need to change any parameters or configure anything, just click the generate button and wait the ~2 minutes for it to generate.

Thanks.

This topic has been closed for replies.

1 reply

ChahinezC
Technical Moderator
July 15, 2022

Hello @DSchu.9​,

I recommend you following the steps described in the 3.3.2 section of the UM1718.

Thank you.

Chahinez.