Skip to main content
VGoya
Associate II
January 12, 2022
Solved

How can we use LwM2M anjay SDK with STM32F4xx series? Is there an example with STM32F4xx?

  • January 12, 2022
  • 3 replies
  • 1429 views

..

This topic has been closed for replies.
Best answer by Peter BENSCH

The Embedded Partner Website of AVSystem says about Anjay LwM2M SDK: 

Anjay is an LwM2M SDK that enables the LwM2M protocol on any hardware device. It features a completely internal implementation of CoAP and is able to run on any kind of platform. The product is released as an open-source and available at: https://github.com/AVSystem/Anjay.

Commercial options which include support and advanced features are also available as a terminator T800.

Probably only AVSystem will be able to help you and tailor the package to a specific target platform.

Regards

/Peter

3 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
January 12, 2022

The Embedded Partner Website of AVSystem says about Anjay LwM2M SDK: 

Anjay is an LwM2M SDK that enables the LwM2M protocol on any hardware device. It features a completely internal implementation of CoAP and is able to run on any kind of platform. The product is released as an open-source and available at: https://github.com/AVSystem/Anjay.

Commercial options which include support and advanced features are also available as a terminator T800.

Probably only AVSystem will be able to help you and tailor the package to a specific target platform.

Regards

/Peter

VGoya
VGoyaAuthor
Associate II
January 17, 2022

Hi Peter,

Thanks you so much..

Please help us on below mention queries:-

Can you please share a link of terminator T800?

Can we interface LwM2M SDK with bare metal device or it required RTOS?

What are the minimum device configuration(Flash size, RAM size, GPIOs etc.) required for LwM2M SDK

Thanks

Vijendra

Peter BENSCH
Technical Moderator
January 17, 2022

Please direct your questions to AVSystem, who will be sure to answer them to your satisfaction.

Regards

/Peter