Visitor II
May 4, 2023
Question
How do I flash firmware to the B-G431B-ESC1?
- May 4, 2023
- 1 reply
- 2443 views
I'm trying to get the basic firmware running, but I think I'm doing something wrong because the ESC doesn't seem to function.
I've generated an IDE project for the B-G431B-ESC1 using the ST Motor Control Workbench, which I then opened in STM32CubeIDE and clicked "Build 'debug' for project" followed by "Run". Everything seems to complete without issues, but when I power the ESC with a 24V supply and give it a PWM signal from a XP3-SSi RC controller the motor doesn't run.
I attached the project's log file, as well as the output from the build and run commands.