How to configure pinout and clock in a project without .ioc file ?
Hello,
I am working with a NUCLEO-F446RE development board and an X-NUCLEO-IHM06A1 motor control board to control a stepper motor.
An example project (STM32CubeExpansion_SPN6) is given with the motor board. However, I want to modify this project to add two PWM outputs and UART communication.
Normally I would do this by modifying the .ioc file, but it is not provided in the example project. Is there any way to recreate the .ioc file? If not, how can I do the PIN configuration? What are the names of the files in which this configuration is found?
Thanks in advance,
Best regards,
Yoan