Skip to main content
Associate III
June 10, 2024
Question

How to get the maximum potential of my engine with MotorControl Workbench_6.3.0?

  • June 10, 2024
  • 2 replies
  • 966 views

Hello.
I am using a Nucleo-F446RE board with the x-nucleo-ihm07m1 driver, to control a LA052-040E servomotor.
Comment that I have not been able to generate the motor profile with the ST Motor Pilot Tool (profiler) V1.2.9.
Which comes with the MotorControl Worbench 6.3.0 program,
After connecting the device and clicking start, the connection is reset and the board is disconnected from the application.

error1.jpg

 

error2.jpg

But with the Motor Profiler 5.4.8 version. Yes, it generates the engine profile for me.

Once the parameters have been entered, the position control application works, but I do not obtain all the desired power.
The current consumed from the supply is 200mA and the motor supports up to 2.5A.
I have the board configured for 1A as the maximum current. 

The driver supports 1.4A constat current.

 

ide.jpg

LA052-040E.jpg

How can I increase the power of the engine, I need it to have more strength. I think he is not giving his full potential.

 

Thank you very much for your help and support.

 

2 replies

Fabrice LOUBEYRE
ST Employee
June 17, 2024

Hi @OttoBCN,

regarding the motor profiler binary, if you generate this MCSDK6.3.0 project with the Hall sensors set as auxiliary sensor, you will face an issue using STM32CubeIde tool. A Hard Fault is generated as soon as you start running the FW with the IDE. You will find below the post with the workaround.

post 

 

 

Best regards.

Fabrice

OttoBCNAuthor
Associate III
June 24, 2024

 

Sorry. I do not know if I explained well.
The motor is configured with the main Observer+PLL sensor. Without enabling the hall sensor or the encoder.

 

OttoBCN_1-1719220435325.png

The program does not work. It is disconnected from the communications port.

Greetings and thanks for your help.