How to resolve PWM timer conflict with NUCLEO-G431RB + X-NUCLEO-IHM07M1 on Linux?
Hi everyone,
I'm new to STM32 and I'm using Debian Linux with the STM32CubeIDE.
I'm trying to use a NUCLEO-G431RB with the X-NUCLEO-IHM07M1 expansion board, using the legacy X-CUBE-SPN7 (apparently the X-Cube-MCSDK is Windows-only...)
I've run into a pin conflict: the expansion board expects the PWM signals on the Arduino standard pins, but on the G431RB those pins are physically connected to separate timers (TIM2, TIM3, TIM8, etc.).
My understanding is that the 6-step libraries (and motor control in general) seem to prefer using a single advanced timer (like TIM1) for synchronization.
Does this timer conflict make sense?
As a last-case scenario, I thought of just connecting both boards using jumper wires (mapping TIM1 outputs to the IHM07M1 inputs) instead of mounting them on top of each other. Is there a known workaround for this?
Thanks!