How to run motor in Open Loop
Hi
I am running on a STM32G071 board, with my own custom HW (standard 3 phase halfbridge). The control is FOC sensorless with 1 shunt
I am having problems tuning the motor, but for starters I would like to run the motor at low speed in open loop
I can find a parameter in the IOC file name Open_Loop_FOC which I can set to "true"
But how do I set the operating conditions and how do I start the motor in Open loop mode?
(I am running MCWB 5.4.1.19309 (I have tried 5.4.4, but it seems to be unstable. STM32CubeIDE 1.4.2 and STM32CubeMX 6.0.1)
Regards
Klaus