Skip to main content
TKara.2
Associate III
July 23, 2025
Question

How to Start Ramp From Actual Speed After Freewheel Mode?

  • July 23, 2025
  • 1 reply
  • 250 views

 

I'm  using button in the MC_APP_PostMediumFrequencyHook_M1 to stop the motor. When I press the button, the motor enters freewheel mode, so it is not actively braked — it simply coasts down.

Later, when I release the button and increase the potentiometer, the motor starts again via a speed ramp. However, I noticed that the ramp always starts from 0 speed, even though the motor was still spinning due to the freewheel behavior.

As a result, the motor gets "locked" momentarily (due to the controller assuming 0 speed), and then accelerates. This is not the behavior I want. Since the motor never truly stopped (freewheel), I would like the ramp to continue from the current actual speed, not from 0.

How can I make the ramp start from the actual mechanical speed of the motor when restarting after freewheel?

__weak void MC_APP_PostMediumFrequencyHook_M1(void)

{

 

uint16_t rawValue = RCM_ExecRegularConv(&PotRegConv_M1);

 

/* USER SECTION BEGIN PostMediumFrequencyHookM1 */

if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_9))

{

MC_StopMotor1();

//HAL_GPIO_WritePin(GPIOC, GPIO_PIN_15, 1);

SpeedPotentiometer_M1.IsRunning =false;

}

 

if(!HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_9))

{

if(rawValue>100)

{

MC_StartMotor1();

}

// HAL_GPIO_WritePin(GPIOC, GPIO_PIN_15, 0);

if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13))

{

SPDPOT_F(&SpeedPotentiometer_M1, rawValue);

}

else

{

SPDPOT_R(&SpeedPotentiometer_M1, rawValue);

}

}

 

bool SPDPOT_R(SpeedPotentiometer_Handle_t *pHandle, uint16_t rawValue)

{

 

bool retVal = false;

 

#ifdef NULL_PTR_CHECK_SPD_POT

if (MC_NULL == pHandle)

{

/* Nothing to do */

}

else

{

#endif

 

SpeednTorqCtrl_Handle_t *pSTC = pHandle->pMCI->pSTC;

 

POT_TakeMeasurement((Potentiometer_Handle_t *)pHandle, rawValue);

SpeednPosFdbk_Handle_t *speedHandle = STC_GetSpeedSensor(pSTC);

if (MCM_SPEED_MODE == STC_GetControlMode(pSTC))

{

if (RUN == MCI_GetSTMState(pHandle->pMCI))

{

 

if (false == pHandle->IsRunning)

{

pSTC->SpeedRefUnitExt = ((int32_t)SPD_GetAvrgMecSpeedUnit(pSTC->SPD)) * (int32_t)65536;

pHandle->IsRunning = true;

 

}

 

if (POT_ValidValueAvailable((Potentiometer_Handle_t *)pHandle))

{

uint16_t potValue = POT_GetValue((Potentiometer_Handle_t *)pHandle);

 

if ((potValue <= (pHandle->LastSpeedRefSet - pHandle->SpeedAdjustmentRange)) ||

(potValue >= pHandle->LastSpeedRefSet + pHandle->SpeedAdjustmentRange))

{

 

int16_t currentSpeed = SPD_GetAvrgMecSpeedUnit(speedHandle);

 

int16_t requestedSpeed = (int16_t)((potValue / pHandle->ConversionFactor) + pHandle->MinimumSpeed);

 

if (currentSpeed < 0)

requestedSpeed = -requestedSpeed;

 

int16_t deltaSpeed = requestedSpeed - currentSpeed;

if (deltaSpeed < 0) deltaSpeed = -deltaSpeed;

 

uint32_t rampDuration = ((uint32_t)deltaSpeed * 1000U) / pHandle->RampSlope;

STC_ExecRamp(pSTC, requestedSpeed, rampDuration);

pHandle->LastSpeedRefSet = potValue;

retVal = true;

}

}

}

else

{

pHandle->IsRunning = false;

}

}

else

{

pHandle->IsRunning = false;

}

 

#ifdef NULL_PTR_CHECK_SPD_POT

}

#endif

 

return retVal;

}

 

 

To solve this, I tried manually assigning the average mechanical speed to the speed reference like this:

STC->SpeedRefUnitExt = ((int32_t)SPD_GetAvrgMecSpeedUnit(pSTC->SPD)) * 65536;

1 reply

Fabrice LOUBEYRE
ST Employee
July 23, 2025

Hi TKara.2,

if you are using the MCSDK6.4.0, you will find the "On The FLy" feature designed for the 6step algorithm. This will allow your motor to restart from a spinning state with no revup phase, as described into the "Six-step Firmware Algorithm" user manual (chapter 5.1.6 Rev-up component and On-the-fly start-up) embedded into the MCSDK Workbench tool.

Please refer to User Manual documentation available through: "Workbench tool">About>Documentations>Documentation>"User manual" tab>"Six-step Firmware Algorithm" link

To enable the feature, you must set the On-the-fly start-up bit into the MCSDK6.4.0 Workbench, and regenerate the project.

FabriceLOUBEYRE_0-1753276791035.png

 

Best regards.

Fabrice