Skip to main content
yang2
Associate III
September 9, 2024
Question

HSO Evaluation Problems

  • September 9, 2024
  • 1 reply
  • 792 views

Dear All,

My platform as list:

Control Board: B-G473E-ZEST1S
Power Board:  STEVAL-LVLP01  

Motor: B-MOTOR-PMSMA1

Platform: MCSDC 6.3.0,  (I attached my Workbench configuration file as follow)

CubeIDE: 1.15.1

 

 

When I try to evaluate the HSO, the Motor pilot appear in weird value.

The speed reference and mechanical speed is wrong.

Also, there are a orange waring, "Access Register of  Bus Voltage resulted in error" on the buttom.

yang2_1-1725866298825.png

 

Once I start the contol, it will occurs "Over Current Fault"

yang2_0-1725866291229.png

 

Has anyone encountered a similar issue? How can it be resolved?

Best Regards,

 

 

    1 reply

    ST Employee
    September 9, 2024

    Hi,

    In fact you are trying to use STOPLL/Cordic UI with a HSO firmware.

    Please load the MC_FOC_ZEST.qml UI instead.

    Thanks

    BRs