HSO Requirement
CURRENT_AMPL_V PC1 ADC1 IN7
Hello
I add a quick look on your stwb6 file.
The issue why you do not see HSO proposed among the Speed Sensing Mode Selection is because of the feature "Phase Voltage Sensing".
This feature is described in your board but the pins connected are the following:
"name": "PC4", -> ADC2
"name": "PA5", -> ADC2
"name": "PA4",-> ADC2
The phase voltage sensing requires at least 2 different ADCs. In your use case only ADC2 is connected.
If you connect one of the 3 signals to an ADC1 pin compatible, then you should see HSO presented by the WB.
Let me know if it is clear and if you succeed to select HSO.
Regards
Cedric
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.